Le damos la bienvenida a Making Waves, donde encontrará historias sobre el agua de Xylem, una empresa mundial de tecnología del agua con la misión de resolver el problema del agua.
Elija artículos y entradas de blog de nuestra selección de temas populares, lea una de las historias destacadas por el equipo de redacción, desplácese por las noticias o seleccione Filtrar por en la barra de navegación superior para acceder a todas las historias y temas de Making Waves. Suscríbase a nuestro boletín mensual para mantenerse al día sobre el maravilloso mundo del agua.
Noticias sobre el agua Sostenibilidad Innovación Cero emisiones Análisis
Historias destacadas del equipo de redacción
All Posts in Water Utilities
Rural North Texas community cuts non-revenue water by 42% with pipeline leak detection technology
In the rural city of Iowa Park, Texas, the Cypress Water Transmission Line serves as a community backbone – delivering drinking water to 6,000 residents and...
More than 90% of global disasters are linked to water, and their impacts are growing. In 2024, floods, storms and droughts caused over $550 billion in economic...
Innovative pumping solution saves energy, expense and space for Großostheim, Germany
The charming Bavarian town of Großostheim, less than an hour southeast of Frankfurt, is home to picturesque streets filled with half-timbered houses and an...
Advanced wastewater treatment in Knoxville gets a UV boost
Flowing through the heart of Knoxville, Tennessee, Beaver Creek is more than just a local waterway – it’s a 303(d) listed stream, meaning it’s been flagged by...
Athens and Los Angeles. These two cities are thousands of kilometers apart, operating in vastly different contexts but pointing in the same direction....
The small town of Clifton, Colorado, is known for its outdoor recreational activities, proximity to local vineyards, and stunning views of the Colorado River....