-
Comunidad de Regantes de Llíria: digitalización integral del regadío para la mejora de la eficiencia y resiliencia operativa
La implantación de una solución integrada, basada en la plataforma Xylem Vue, ha permitido a la Comunidad evolucionar hacia una gestión digital, centralizada y en tiempo real del sistema. -
Giahsa: Supervision and control of the sanitation network
Improve control, responsiveness, and efficiency of facilities and processes by providing real-time network status information and analyzing historical network and asset data. Increase resource management effectiveness and efficiency to provide customers with the highest level of service at the lowest possible cost.
-
Aguas de Calpe: Smart management of the drinking water and sanitation system
As a municipality with significant fluctuations in water consumption—extremely high demand during the summer—that also relies on multiple reservoir and pumping stations to deal with issues associated with its complicated terrain, the town of Calpe, Spain wanted to optimize their water cycle management.
-
Servicios de Agua Drenaje de Monterrey: Reducing non-revenue water and controlling pressure
Regulate and monitor pressures, supervise flow rates, consumption, and non-revenue water (NRW) in different sectors, and bring together system information from various sources including the SADM’s SCADA.
-
Triple A Barranquilla: Controlling water loss and integrating water system management
Improve hydraulic efficiency of the water distribution system for the City of Barranquilla, Colombia and its 14 surrounding municipalities and reduce non-revenue water losses, which were around 50%.
-
CCACVI: Acquisition, implementation, hosting and maintenance of a hypervision solution for water and sanitation systems
The French Community of Communes Albères Côte Vermeille Illibéris (CCACVI) is promoting a hypervision project to streamline its water cycle, based on the Xylem Vue platform. -
Government of the Principality of Asturias: implementation of a DataHub for regional water cycle management
The solution was set up as a regional DataHub based on the Xylem Vue platform, and provides a comprehensive, centralized view of the regional water cycle to accelerate decision-making. -
CGUCJT: decision-support system for the Jucar-Turia Canal irrigation system
The implementation of Xylem Vue’s Agrotwin platform has enabled the CGUCJT to transition to digital, centralized, real-time management of the Jucar-Turia Canal’s main irrigation water delivery system. -
Ciudad de Mánchester: Captura y reutilización eficiente de aguas pluviales a través de datos y análisis
El Manchester City FC utiliza tecnología inteligente y reutilización de aguas pluviales para reducir el uso de agua potable en su campus Etihad. Con la ayuda de la plataforma basada en datos de Xylem, el club tiene como objetivo optimizar la irrigación y lograr una reutilización completa de las aguas pluviales para 2026.
-
Brabant Water: end-to-end advanced water supply digitalization using Xylem Vue
Brabant Water deployed Xylem Vue to digitalize its network, integrating data for near real-time operational intelligence and non-revenue water management. -
Realtime monitoring cuts pollution risk at Scottish Water site
When a critical pumping station failed, Scottish Water used Xylem Vue Secure Connect monitoring and real-time data to restore resilience and protect the environment. -
ESAMUR: plataforma de digitalización integral para la supervisión avanzada de los sistemas de depuración en la Región de Murcia
El proyecto REGEN-IA, articulado sobre la plataforma Xylem Vue, tiene como objetivo integrar, gobernar y explotar la información operativa de ESAMUR en un único entorno. -
Mimizan: reducing inflow and infiltration through centralized data collection and analysis
The Mimizan Federation of Municipalities is implementing the Xylem Vue platform to reduce inflow and infiltration by improving infrastructure monitoring. -
Redland city council: Cleveland WWTP operational improvement & data management project with Xylem Vue platform
Redland City Council unified plant operations data with Xylem Vue, boosting compliance monitoring and efficiency at Cleveland WWTP. -
Severn Trent Water: digital twin to optimise energy and emissions in WWTPs
The implementation of a digital twin at the Strongford treatment works has enabled Severn Trent Water to visualise plant performance in near-real time. -
EMALCSA: implementación de un gemelo digital para apoyar la toma de decisiones en la operación de la red de abastecimiento
La Empresa Municipal de Aguas de La Coruña (EMALCSA) gestiona el ciclo integral del agua en la ciudad de A Coruña y en otros siete municipios cercanos, con una población total de 400.000 habitantes. La operadora española capta, potabiliza y distribuye más de 36 millones de metros cúbicos de agua potable a 138.000 clientes cada año, a través de una red de más de 560 kilómetros, 26 depósitos y seis estaciones de bombeo. -
ALJARAFESA: gestión avanzada de activos y movilidad del ciclo integral del agua
Descubra cómo ALJARAFESA modernizó las operaciones del ciclo del agua mediante una plataforma digital unificada que conecta la gestión de activos, el mantenimiento y la detección de fugas para mejorar la eficiencia, la capacidad de respuesta y la prestación del servicio. -
Orekan (Gobierno de Navarra): Sistema de Alerta Temprana para reducir el riesgo de inundaciones
La Comunidad Foral de Navarra, situada en el norte de España, cuenta con una superficie de más de 10.000 km² y una población aproximada de 680.000 habitantes, concentrada principalmente en el entorno metropolitano de Pamplona. Su territorio presenta una elevada complejidad hidrológica, al estar dividido entre la cuenca del Ebro, que abarca aproximadamente el 90% de la comunidad, y la vertiente cantábrica, caracterizada por cuencas cortas y de respuesta rápida. -
CABB: optimization of the primary wastewater network
The Bilbao Bizkaia Water Consortium (CABB) is the public utility responsible for managing the main drinking water and wastewater network in the province of Bizkaia, serving over one million residents through a range of water supply pipelines, sewer networks, and wastewater treatment plants across 97 municipalities. -
EMASESA: implantación de un gemelo digital del abastecimiento y saneamiento para optimizar la toma de decisiones
Implantación de la plataforma Xylem Vue con el objetivo de optimizar la gestión, anticipar eventos y mejorar la eficiencia, resiliencia y sostenibilidad del ciclo integral del agua en Sevilla. -
Gruppo CAP: gestión inteligente de la red de abastecimiento mediante analítica avanzada y planificación predictiva de activos
Gruppo CAP implementó Xylem Vue para optimizar su red de agua de 6.500 km, reduciendo pérdidas y mejorando la gestión de activos. -
Real-time decision support helps cut combined sewer overflow volume by 100 million gallons and reduces capital needed for regulatory compliance
Evansville is located on the north bank of the Ohio River in southwest Indiana. The City’s sewer system, parts of which are more than 100 years old, serves a population of 163,000, with combined sewers making up almost 40 percent of the total sewer area.
-
Global Omnium: Transforming from Conventional to Smart Water
Global Omnium, one of Spain's largest water utilities, has gone through a remarkable digital transformation over the past two decades - upgrading from conventional meters to an advanced smart meter network of over 550,000 fixed network smart meters. This journey provides valuable lessons for any water utility looking to modernize its operations and capitalize on the latest innovations in smart metering and data analytics.
-
EMASA: Incremento de la eficiencia hídrica a partir del análisis inteligente del balance hidráulico
EMASA (Empresa Municipal Aguas de Málaga S.A.) es la empresa pública del Ayuntamiento de Málaga encargada de la gestión integral del ciclo urbano del agua desde 1987. La entidad presta servicio a más de 600.000 habitantes y distribuye aproximadamente 42 hm³ de agua potable. El sistema opera con un caudal de hasta 2 m3/s por segundo, asegurando el abastecimiento urbano a través de una extensa red que alcanza casi 2.000 km de tuberías, está sectorizada en alrededor de 240 DMA y cuenta con más de 240.000 contadores, de los que 170.000 son smart meters.