-
ARA Pustertal AG: reducing aeration energy consumption by 10% in a WWTP thanks to a digital twin
ARA Pustertal AG operates the Innichen-Sexten wastewater treatment plant (WWTP) in the South Tyrol area of Italy. The plant, which has a capacity for 36,000 inhabitants, uses a conventional activated sludge process, with pre-denitrification and biological phosphorus removal.
-
Immokalee Water & Sewer District: deployment of a comprehensive water management solution
The Immokalee Water and Sewer District was set up in 1978 to provide affordable, reliable water and sewer services to Immokalee, an unincorporated area of Collier County, Florida. The district operates and maintains the water and sewer plants and systems as an Independent Special District of the State of Florida, serving more than 24,000 year-round residents.
-
Stadtwerke Trier: optimization of wastewater treatment plant processes thanks to AI
Stadtwerke Trier (SWT) operates the main wastewater treatment plant (WWTP) in Trier, with a capacity of 170,000 population equivalents. This facility was one of the largest energy consumers in the utility for many years, with hundreds of thousands of kilowatt hours of valuable energy being drawn from the public grid as a result of poor control.
-
Metro Water Services: deploying a digital twin to manage drinking water distribution in real time
Nashville’s city government has a deep-rooted history in the water industry, providing drinking water to its citizens since the early 1800s. Today, Nashville Metro Water Services (MWS), Tennessee, serves more than 191,000 customers in Nashville and surrounding counties.
-
Taron™ Activated Sludge Filter Provides Effective Total Suspended Solids (TSS) Reduction
For Pennsylvania’s Western Butler County Authority (WBCA), peak flow events due to inflow and infiltration (I&I) have gone hand-in-hand with aging sewage system and treatment plant infrastructure.
-
Consorcio de Aguas de Tarragona: implementación de una solución avanzada de gestión de datos
El CAT implementó la plataforma Xylem Vue y su Smart Water Engine para resolver este problema e impulsar la eficiencia hídrica y energética. La aplicación Unified Network Management se implementó para proporcionar un único centro de control para los activos de tratamiento de agua potable, independientemente de su ubicación geográfica.
-
Taron™ activated sludge filter delivers needed capacity to meet discharge limits
A food processing company’s wastewater treatment plant was struggling to meet local discharge limits and faced a hard deadline for compliance from the local authority. The problem centered on excessive solids in the effluent. To ease the hydraulic load on the existing concrete secondary clarifier and reduce total suspended solids (TSS), Xylem installed a Taron activated sludge filter.
-
An innovative project in Neustadt in Holstein
Faced with high standards for both efficiency and sustainability, Averdung and the municipal utility sought a partner capable of realizing this supply through seawater source heat pumps using Baltic Sea water.
-
Bremen's Future District: Sustainable Energy from the River
The investor set out to realize a sustainable and innovative concept that meets the demands of a contemporary urban quarter.
-
BALTEN: Implementation of an advanced business management system (ERP)
BALTEN needed to modernize its outdated infrastructure and software platforms, so it could optimize its irrigation water transportation system and improve the overall performance of its irrigation water service.
-
Xylem CoMag helps Yorkshire Water exceed phosphorous targets
Due to a projected population increase, discharges from the site were required to undergo advanced biological treatment to reduce levels of phosphorous returned to the River Aire. This requirement was part of the UK Environment Agency’s Water Industry National Environment Programme (WINEP).
-
La CHE mejora la prevención y gestión de inundaciones en la cuenca del Ebro
La Confederación Hidrográfica del Ebro (CHE) ha desplegado un sistema de alerta temprana para anticipar crecidas fluviales, inundaciones pluviales y riadas repentinas en toda la cuenca del Ebro (85.000 km²), integrando datos de sensores hidrológicos y meteorológicos, radar de precipitaciones y modelos de predicción meteorológica para ofrecer alertas, mapas y recomendaciones operativas a tiempo.
-
State of the art water treatment technology for a German outdoor pool in Bernsbach
The operators wanted to use non-hazardous table salt with electrolysis for disinfection. They were also looking for a filter technology that generates low wastewater costs and can be installed in a space-saving manner.
-
Safeguarding water supplies with SmartBall
In 2020, real water loss in the town’s network peaked at 27 percent. Leaks were undermining the town’s critical water conservation efforts. Recognizing the urgency of the issue, the town is deploying innovative solutions to combat water loss and ensure a sustainable water supply.
-
Risks associated with the use of dispense gases in a food and beverage service establishment
A dispense gas is simply a pressurized gas used for dispensing drinks. The gas of choice is typically carbon dioxide (CO2), especially for carbonated drinks such as soda and beer. Carbon dioxide is commonly employed in the food service environment in a variety of equipment systems such as carbonation, refrigeration, and....
-
Buffalo Sewer Authority: wet weather operational optimization and real-time control system
As the level of national awareness for the need to protect our nation’s water resources continued to grow, federal and state regulators pursued a consent decree in 2006 requiring enhancements to Buffalo’s collection system.
-
Dŵr Cymru Welsh Water, Hirwaun Water Treatment Works, Glamorgan
Dŵr Cymru Welsh Water’s Hirwaun water treatment works is a small works (5Ml/d) which treats raw water from the Penderyn upland reservoir. Treatment is by coagulation with ferric sulphate and lime, flocculation and clarification by DAF. The clarified water is dosed with lime and this is followed by first stage filtration in four rapid gravity filters, intermediate electrochlorination and orthophosphoric acid dosing, and second stage filtration in four pressure filters. Final disinfection is by electrochlorination. The original electrochlorination plant was an Evoqua OSEC® packaged unit installed over twenty years ago and had reached the end of its asset life.
-
Fighting Water Loss: Best Practices to Reduce Non-Revenue Water and Operate Sustainably
Learn best practices for leak detection, pressure management, and smart metering to help utilities address Non-Revenue Water and move toward a more sustainable "watertight" future. This guide offers practical solutions and valuable insights to create a more efficient and equitable water infrastructure.
-
Our 15 most frequently asked questions on improving aquaculture
To help companies protect against waterborne infection and disease, Evoqua recently hosted a webinar dedicated to understanding and improving water quality in land-based hatcheries that you can watch here.
-
-
City of Tulare celebrates 25 years of converting waste-to-energy
The City of Tulare, located in California’s world renowned San Joaquin Valley, is known for its rich agricultural and dairy industries. Tulare is home to six large-scale cheese and dairy producers. Like many municipalities, the city is challenged to meet industrial requirements at a reasonable cost while maintaining harmonious relationships with the surrounding community.
-
CoMag® System Provides Immediate Results
Situated in Staffordshire in the UK, the Severn Trent Cannock wastewater treatment facility serves a population of 65,053. The plant had early obligation AMP7 requirements to meet for controlling phosphorus levels.
-
Community with poor soil conditions seeks safe, chemical-free solution
The Fredericksburg Sewer & Water Authority (FSWA) owns and operates two wastewater treatment plants, five wastewater pumping stations, three wells and three water storage facilities.
-
Cover helps community control odors from wastewater treatment
When the affluent, new home development was being established, odor control was top of mind. The wastewater treatment plant was in close proximity to the new development, which includes 900 acres (364 hectares) of preserved open space, including 24 miles (38 kms) of trails, 10 neighborhood parks, a community pool and water park, as well as outdoor sport courts.