It looks like you are coming from United States, but the current site you have selected to visit is Equatorial Guinea. Do you want to change site?

Yes, please! No, keep me on the current site

Enable high contrast mode

Cost-efficient pump station

BELGIUM

Challenge

To provide a cost-efficient pump station fed by three independent inlets, resulting in a potential maximum inflow of 7.8 m3/s (123,000 US gpm) combined. Air entrainment into the pumps due to the three independent inlets presented challenges.

Solution
We designed a solution using four Flygt PL 7101 propeller pumps with a total capacity of 8 m3/s (127,000 US gpm). This solution is shallower than competitors’ solutions and has a lower height for lifting the water, which reduces energy consumption. The design was verified through physical hydraulic scale model tests to ensure the reliability of the solution.